메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why source file cannot be found in <project folder>/src,?

Latest Updated:03/08/2016

Question:

When a source file is created or moved out of <project folder>/src, the file is not compiled.

Answer:

"Source location folder" setting is defined with 'project folder'/src by default. To add souce codes in other folders please follow the procedure below.

  1. Open "Paths and Symbols" dialog through the menu of "Project" -> "Properties",
    then choose "C/C++ General" -> "Path and Symbols" in category tree.
  2. Select "Source Location" tab.
  3. Press [Add Folder...] button and browse for a new source file location. To specify 'project folder', please choose ".".
Suitable Products
e² studio
  • 이 기사가 도움이 되셨나요?