메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

e² studio archived project failed to build

Last Updated:06/28/2017

Question:

I have imported an archived e² studio project, but it failed to build. Why?
cf. Why the context is invisible in sample code (Runesas Rulz)

Answer:

If the project refers to source files or header files out of the project folder (for example, files in the “bleip” and “rBLE” folders, and sub folders of “renesas”, as shown below), you need to import those files, too.
In such cases, you should once extract and then import the project, not as “archive”.
This project refers to files in above folders.

Note that, before pressing the [Finish] button, you also need to uncheck the “Copy projects into workspace” option.

Suitable Products
e² studio
  • 이 기사가 도움이 되셨나요?