메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Bluetooth Specification Version of Product Implementing RL78/G1D

Last Updated:02/05/2018

Question:

What is the Bluetooth specification version of a product that implements the RL78/G1D or RL78/G1D module (RY7011)?

Answer:

The Bluetooth specification version of the end product is "4.2" as the core specification version supported by the core (protocol) stack, installed in the RL78/G1D and RL78/G1D module (RY7011), is applied.
Details of core stack can be confirmed with Launch Studio of Bluetooth SIG below.
https://launchstudio.bluetooth.com/ListingDetails/10444
Suitable Products
RL78/G1D
Bluetooth
  • 이 기사가 도움이 되셨나요?