메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Public Device Address for products with Bluetooth low energy technology

Last Updated:02/13/2017

Question:

Is an assigned "Public Device Address" required to sell products with Bluetooth low energy technology?

Answer:

If using a "Random Device Address", the "Public Device Address" is not absolutely necessary. However, care should be taken because the "Random Device Address" may be duplicated possibly causing undesired operation.
Suitable Products
RL78/G1D
Bluetooth
  • 이 기사가 도움이 되셨나요?