메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can a parameter sheet be issued?

Latest Updated:12/01/2006

Question:

It is said that a parameter sheet is necessary for exporting from Japan. Can it be issued?

Answer:

Refer to "Kohyo list (Declared List)" of CISTEC. If the product is listed there, submitting an individual parameter sheet is unnecessary. Write the release date on the invoice to clear customs for export.

CISTEC's "kohyolist (Declared List)" can be purchased from CISTEC.
CISTEC's contact information is listed below.

Center for Information on Security Trade Control (CISTEC)
New Toranomon Jitsugyo Kaikan 4F 1-1-12 Toranomon, Minato-ku, Tokyo, Japan 105-0001
Tel: +81-3-3593-1147
Fax: +81-3-3593-1136
http://www.cistec.or.jp/english/index.html
Suitable Products
  • 이 기사가 도움이 되셨나요?