메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How is microcontroller judged with the Japanese Trade Control Act?

Latest Updated:11/01/2005

Question:

How must it be judged if a microcontroller is in compliance with the Japanese Trade Control Act?

Answer:

Mask ROM microcontrollers and written one-time programmable (OTP) microcontrollers cannot have their programs rewritten, so users designing their own program specifications must judge if the microcontroller is in compliance with the act.
When the user makes the judgment, the parameter sheet is classified as a dedicated integrated circuit (integrated circuit designed to be used for a specific system).
Please consult a Japanese sales representative or distributor for further questions.
Suitable Products
  • 이 기사가 도움이 되셨나요?