메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do the lead-free products differ from those of conventional products?

Latest Updated:11/01/2007

Question:

Do the soldering conditions for lead-free products differ from those of conventional products?

Answer:

In general, it is different. But some conventional products meet the lead-free soldering conditions.
For the soldering conditions of lead-free products, refer to Lead-free Semiconductor Product Pamphlet.
For the soldering conditions of each product, either refer to their respective data sheets, or ask to the distributor.
Suitable Products
  • 이 기사가 도움이 되셨나요?