메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What does Failure Rate (λ) mean?

Latest Updated:08/01/2005

Question:

Failure Rate (λ)

Answer:

Fit is used as a unit, which stands for Failure in time.
It describes the rate of failure in a given time period and can be expressed as 1 FIT = 1 x 10-9/hour.

A failure rate is an estimate value and varies depending on the operating conditions (voltage, duty, etc.) and environment (temperature, humidity, etc.) of the customer.

For details, refer to the Review of Quality and Reliability Handbook.
Suitable Products
  • 이 기사가 도움이 되셨나요?