메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What happens if the digital output current differs from rated values?

Latest Updated:04/01/2008

Answer:

For general-purpose ports with phased current value ratings, you can analogize using Ohm's Law (H output falls below VDD, L output rises above GND). Note that for some microcontrollers, the characteristics graphs (reference values) are available on our website .
However, since the output current conditions (maximum value when phased ratings are used) assume the maximum load, don't pass a rated current because this may degrade the reliability of the semiconductor device.
Suitable Products
  • 이 기사가 도움이 되셨나요?