메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Which is the pin 1 mark on the surface of the chip?

Latest Updated:08/01/2005

Question:

On the surface of the chip I can see circular white markings and stamp depressions: which is the pin 1 mark?

Answer:

The double circle is the pin 1 index. Painted markings or laser markings indicate that the product is lead (Pb) free.
Suitable Products
  • 이 기사가 도움이 되셨나요?