메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can PSW ID flag control be performed and operate by the user?

Latest Updated:12/01/2011

Question:

Can PSW ID flag control be performed by the user?
Is a system call provided to operate the PSW ID flag?

Answer:

This is managed by the OS. Do not manipulate this within the OS.
Suitable Products
  • 이 기사가 도움이 되셨나요?