메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Conditions of the HALT status is entered other than memory shortage

Latest Updated:12/01/2011

Question:

Control shifts to the initial block of the nucleus and the HALT status is entered.
Are there any conditions under which this will happen other than memory shortage?

Answer:

The OS enters the HALT status when a management table cannot be created for some reason, rather than due to memory shortage.
In addition, check to make sure there is no program lockup or memory error.
Suitable Products
  • 이 기사가 도움이 되셨나요?