메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How many clocks does it take to perform DI?

Latest Updated:12/01/2011

Question:

Is there any processing other than using the clock handler to perform DI, such as using an OS system call?
In this case, how many clocks does it take to perform DI ?

Answer:

DI processing is performed in various places within the OS such as task scheduling.
However, it is generally expressed in units of time limited to the CPU and operating clock (not calculated by the number of clocks).
Suitable Products
  • 이 기사가 도움이 되셨나요?