메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(E1, E21)Is level of difference between actual and nominal baud rates a problem?

Latest Updated:12/01/2011

Question:

Since the baud rate is determined by division of the internal clock, the actual baud rate varies slightly from the nominal value of the baud rate.
For example, when inputting a 16MHz or 32MHz clock, there is a difference of 0.16%. (Nominal value: 9600bps; Actual value: 9615bps)
Is this level of difference between the actual and nominal baud rates a problem?

Answer:

In normal cases, this variation should not be a problem.
For normal UART, the margin is approximately 45% of the bit length.
When this is divided by the total bit length, the figure is a little under 4%, and even if the transmitting side and the receiving side consume half of this figure,
it is a little under 2%. Thus 0.16% is not at all a problem.
Suitable Products
RL78 Family
78K Family
  • 이 기사가 도움이 되셨나요?