메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

About RAM-ECC function (on-chip debugger is enabled)

Last Updated:01/16/2018

Question:

Is the RAM-ECC function enabled when the CPU is activated in normal operation mode while the on-chip debugger is enabled by the on-chip debug option byte?

Answer:

The RAM -ECC function is enabled when the CPU is activated in normal operation mode (the CPU is not connected to the on-chip debugger) even if the on-chip debugger is enabled.
Suitable Products
RL78/F13
RL78/F14
RL78/F15