메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

About data retention years of flash memory (per block)

Last Updated:01/16/2018

Question:

The number of times that flash memory can be rewritten is specified for each block. If one block of the data flash memory is erased 100,000 times and another block of the data flash memory is erased 1,000 times, is the data retention period different between the two blocks?

Answer:

The data retention period is also specified for each block. Accordingly, the period (years) varies if a different period is specified for the relevant blocks.
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/D1A
RL78/G13
RL78/G14
  • 이 기사가 도움이 되셨나요?