메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

When a reset occurs due to the watchdog timer, does the same operation as /RESET pin input result?

Last Updated:12/26/2017

Question:

When a reset occurs due to the watchdog timer, does the same operation as /RESET pin input result?

Answer:

Yes, this is correct.
For details, refer to the "Reset Function" section in the User's Manual.
Suitable Products
RL78 Family
78K Family