메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Interference when input pins & output pins are mixed w/ output pin side?

Latest Updated:12/01/2011

Question:

In the uPD780308, when input pins and output pins are mixed in the same port and the on-chip pull-up resistor is set to ON, does this cause interference with the output pin side?

Answer:

No, this does not cause interference. (There is no problem.)
As can be seen in the port block diagram, the pull-up resistor of each port can only be enabled by setting the PUO register to 1 and also setting the PM register to 1 (in other words, input port mode).
Therefore, no pull-up resistor can be connected to a pin specified as output.
Suitable Products
RL78 Family
78K Family
  • 이 기사가 도움이 되셨나요?