메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why the LEDs connected to ports light upon reset? How can I prevent it?

Latest Updated:12/01/2011

Question:

The LEDs connected to the ports light upon reset. What is the cause and how can I prevent it?

Answer:

At reset, all the ports enter the input mode (high-impedance status).
When TTL is used for the external buffer, there is a high likelihood that the high-impedance status will be judged as a high level.
If the circuit is designed so that LEDs light when the port outputs are high level, the LEDs will light as a result.

The handling to prevent this is to make the LEDs light when a low level is output.

Suitable Products
RL78 Family
78K Family
  • 이 기사가 도움이 되셨나요?