메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(RX210) Module stop control register can't be set. Any special setting needed

Latest Updated:06/10/2013

Question:

The module stop control register cannot be set. Is any special setting required?

Answer:

This product has a register write protection function that protects important registers from being rewritten. To perform settings to a protected register, writing must first be enabled by the above function.

Please refer to the application note "Register Write Protection Setting Example" (R01AN1206EJ) for details on the register write protection function.

 

Suitable Products
RX210
  • 이 기사가 도움이 되셨나요?