메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can A/D conversion be performed on other analog input?

Latest Updated:05/20/2014

Question:

When temperature sensor output or internal reference voltage is selected as the target of the A/D converter, can A/D conversion be performed on other analog input?

Answer:

No. When temperature sensor output or internal reference voltage is selected, please select single-scan mode, remove all analog inputs from conversion target, and perform A/D conversion.
Suitable Products
RX630
RX63N, RX631
RX210
RX21A
RX220
RX110
RX111
  • 이 기사가 도움이 되셨나요?