메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I rewrite a program from boot mode using the synchronous comm.?

Latest Updated:01/23/2014

Question:

Is it possible to rewrite a program from boot mode using asynchronous communication?

Answer:

It is possible. In boot mode, the built-in serial communications interface is used for communication in asynchronous mode between the host and the microcontroller.
Suitable Products
RX630
RX63N, RX631
RX210