메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can a DMACA activation be received during DTC transfer?

Latest Updated:06/20/2013

Question:

Can a DMACA activation be received during DTC transfer?

Answer:

The activation source is pended until after the current DTC operation has completed. At this time DMACA arbitrates for usage of internal main bus 2 to complete the pending request.
Suitable Products
RX62N, RX621
RX62T
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111
  • 이 기사가 도움이 되셨나요?