메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Effect of Crystal Oscillation Variations

Last Updated:06/08/2017

Question:

The operating frequency exceeds the recommended operating conditions due to oscillation variations with the crystal.  Will this cause any problems?

Answer:

If the operational frequency is exceeded due to oscillation variations, it will not affect MCU operations.
Suitable Products
RX Family
  • 이 기사가 도움이 되셨나요?