메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

External clock: is it necessary to connect resistance in EXTAL & XTAL?

Latest Updated:06/20/2013

Question:

When inputting an external clock, is it necessary to connect resistance between EXTAL and XTAL?

Answer:

It is not necessary.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111
  • 이 기사가 도움이 되셨나요?