메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

High-Speed Operation Problems with RSPI

Last Updated:06/08/2017

Question:

Communications do not operate properly when the RSPI bit rate is set to high speed. Where should I check to fix this?

Answer:

You need to check the terminal setting used for RSPI. Check the setting of the “DSCR” drive capacity control register and select “High-drive output” for all the terminals which can be set to "high drive", and try again.

However, products that do not have the drive capacity control register "DSCR" are not included. (Target products: RX610 group, RX62T group, RX62G group)

Suitable Products
RX Family
  • 이 기사가 도움이 되셨나요?