메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to execute a program without changing the state of the MD or PC7 pin?

Latest Updated:06/10/2013

Question:

After rewriting the user area in user boot mode, is it possible to then execute a program which is in the user area without changing the state of the MD pin or PC7 pin?

Answer:

Yes, it is possible. However, since the operating mode would still be user boot mode, there will be some restrictions, such as not being able to enter software standby mode or deep software standby mode.
Suitable Products
RX210
  • 이 기사가 도움이 되셨나요?