메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

In clock synchronous mode, is it possible to invert the clock or delay?

Latest Updated:01/23/2014

Question:

In clock synchronous mode of the serial communications interface, is it possible to invert the clock or delay by half a clock?

Answer:

It is possible if simple SPI mode is used. For details, please see Operation in Simple SPI Mode in the User's Manual: Hardware.
Suitable Products
RX630
RX63N, RX631
RX210
  • 이 기사가 도움이 되셨나요?