메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the signal inputs to the three functions of PF as it enables?

Latest Updated:05/27/2013

Question:

When port function (PF) is used to enable three peripheral functions, is a signal input to these three functions?

Answer:

A signal is input to all three enabled peripheral functions.
Suitable Products
RX62N, RX621
RX62T
RX610
  • 이 기사가 도움이 되셨나요?