메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the programming software used with RX62N USB boot?

Latest Updated:09/15/2011

Question:

What is the programming software used with RX62N USB boot?

Answer:

The only software (programmer) that runs with RX62N USB boot is the Flash Development Toolkit.
The USB boot driver cannot be provided.
Suitable Products
RX62N, RX621
  • 이 기사가 도움이 되셨나요?