메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

RTC function (RX62N Series): Importance of a crystal resonator?

Latest Updated:05/27/2013

Question:

In the Realtime Clock (RTC) chapter of the RX621/62N Group User's Manual: Hardware, there are mentions of "connecting a crystal resonator" and "has a...crystal resonator".

If I want to use the RTC function of the RX62N Series, is it necessary to connect a crystal resonator? Or is it not necessary?

Answer:

In the RX62N Series user's manual: hardware, "has a...32.768-kHz crystal resonator" means that the device has an oscillation circuit that oscillates on a connected crystal oscillator.
To perform RTC operation, it is necessary to connect a 32.768-kHz crystal resonator between the XCIN and XCOUT pins.

 

Suitable Products
RX62N, RX621
  • 이 기사가 도움이 되셨나요?