메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What are other information on the protection of on-chip flash memory?

Latest Updated:06/20/2013

Question:

I need more information on the protection of on-chip flash memory.

Answer:

There is a protect function for preventing readout/writing/erasing of the on-chip flash memory.
In order to perform readout/writing/erasing, the following registers need to be set correctly.
- FENTRYR.FENTRY0 to 3 bits
- FENTRYR.FENTRYD bit
- DFLWEy register
- DFLREy register
- FWEPROR.FLWE[1:0] bit

For information on the protect function that prevents third-party access to the on-chip flash memory, please refer to the application note "RX Family/RX600 Series Forbidding Third-Party Access to the On-chip Flash Memory".

Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210
  • 이 기사가 도움이 되셨나요?