메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is on-chip ROM (user boot) (read only)?

Latest Updated:12/19/2013

Question:

What is on-chip ROM (user boot) (read only)?

Answer:

The on-chip ROM (user boot) (read only) area is where programs are executed in user boot mode. To write to this area, use boot mode.
For more information, please refer to the "User Boot Mode" section in the "ROM (Flash Memory for Code Storage)" chapter of the hardware manual.
Suitable Products
RX62T
RX610
RX62G
RX210
  • 이 기사가 도움이 되셨나요?