What is single write strobe mode appears in Buses chapter in manual?
Latest Updated:06/20/2013
Question:
What is the single write strobe mode that appears in the Buses chapter of the hardware manual?
Answer:
Single write strobe mode selects which control signals are used when accessing external memory (16bits width). It is defined in Section 11.3.3 of the HW manual.
Suitable Products
RX62N, RX621 |
RX610 |
RX63T |