메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the reference voltage of the A/D converter of RX62T Group?

Latest Updated:05/27/2013

Question:

There is no VREF pin on the 80-pin package of the RX62T Group. What is the reference voltage of the A/D converter in this case?

Answer:

In the 80-pin package, VREF is connected to AVCC internally. Therefore, the voltage supplied to the AVCC pin is the reference voltage of the A/D converter.

 

Suitable Products
RX62T
  • 이 기사가 도움이 되셨나요?