메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the status of the pins during reset and standby?

Latest Updated:06/20/2013

Question:

What is the status of the pins during reset and standby?

Answer:

Please refer to the Appendix "Port States in Each Processing Mode" of the hardware manual.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111
  • 이 기사가 도움이 되셨나요?