메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does the DDR interface (DDRI/F) of the RZ/G1E support 16-bit?

Latest Updated:05/09/2016

Question:

Does the DDR interface (DDRI/F) of the RZ/G1E support 16-bit?

Answer:

Yes. When using 16-bit, please connect DRAM to DRAM0 (M0DQ0 to 15).
Suitable Products
RZ/G1E
  • 이 기사가 도움이 되셨나요?