메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How many levels of USB hubs can be connected in cascade to one USB 2.0 host port?

Latest Updated:05/09/2016

Question:

How many levels of USB hubs can be connected in cascade to one USB 2.0 host port?

Answer:

As per the USB specifications, up to 5 levels of hubs can be cascaded together.
Suitable Products
RZ/G
  • 이 기사가 도움이 되셨나요?