메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are there any precautions when using the PCMCIA interface?

Latest Updated:03/23/2009

Question:

Are there any precautions when using the PCMCIA interface?

Answer:

1) The PCMCIA interface of SH-4 supports only little endian. Please use SH-4 in little endian when using the PCMCIA interface.

2) WAIT cycle setting during bus access depends on "ON" or "OFF" of MMU.

Suitable Products
SH7751R
SH7751
SH7750S
SH7750R
  • 이 기사가 도움이 되셨나요?