Can data MAT in data flash be kept when rewriting on-chip flash memory?
Latest Updated:09/11/2012
Question:
Can the content of the data MAT in the data flash (FLD) be kept when rewriting the on-chip flash memory (User MAT) in the user program mode?
Answer:
The data in the data flash (FLD) will be kept during execution of the user program mode.
Suitable Products
SH7214, SH7216 |
SH7231 |
SH7239, SH7237 |