메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can each capacity of cache and RAM built in the SH7727 be shared?

Latest Updated:03/25/2009

Question:

Can each capacity of cache(16KB) and RAM(16KB) built in the SH7727 be shared?

Answer:

Since the cache and built-in RAM of the SH7727 are independent modules, they can not share their capacity mutually.
Suitable Products
SH7727
  • 이 기사가 도움이 되셨나요?