메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does SH operate improperly if set up time of WAIT signal not kept?

Latest Updated:03/25/2009

Question:

When the setup time or the hold time of the WAIT signal is not kept, does SH operate improperly?

Answer:

Even if the setup time or the hold time of the WAIT signal is not kept, SH does not operate improperly.However, the wait cycle may not be inserted.
Suitable Products
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7032
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017