메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does the SDRAM possible to be used as display memory for LCD?

Latest Updated:03/24/2009

Question:

Is only the synchronous DRAM (SDRAM) possible to be used as display memory for LCD?

Answer:

When using LCD controller, the display memory supports only the
synchronous DRAM (SDRAM) connected to the area 3.
Suitable Products
SH7727
SH7720
  • 이 기사가 도움이 되셨나요?