From which cycle is data outputted in the extension of CS assert term?
Latest Updated:03/23/2009
Question:
Regarding the operation in the extension of CS assert term, when CS assert additional extension is carried out in the setup of address /data multiplexer I/O space, which cycle is the data outputed from?
Answer:
SH7065=>The writing data is output from the Th cycle.
Except the above => The writing data is output from the T1 cycle.
Suitable Products
SH7065 |