메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How data bus operate when access in 16/32 bits to external memory space where 8 bit bus width is set,?

Latest Updated:03/26/2009

Question:

When accessing in the word size(16 bits) or longword size(32 bits) to the external memory space where 8 bit bus width is set, how will the data bus operate?

Answer:

If 8 bit bus width is set, the effective data bus will be D7~D0 pins regardless of the access size of longword/word/byte.
The data is output to D7~D0 pins as follows, when accessing in the word size(16 bits) or longword size(32 bits) to the external memory space where 8 bit bus width is set.

When accessing to Address n in the longword size, 4 consecutive memory accesses are generated.

  • 1st access Address n
  • 2nd access Address n+1
  • 3rd access Address n+2
  • 4th access Address n+3

When accessing to Address n in the word size, 2 consecutive memory accesses are generated.

  • 1st access  Address n
  • 2nd access Address n+1
Suitable Products
SH7144, SH7145
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017