메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to process HIFMD pins when the host interface function is not used?

Latest Updated:03/23/2009

Question:

How should be processed the HIFMD pins when the host interface function is not used?

Answer:

Because the HIFMD function is selected as for an initial value, the pin processing is necessary though the HIFMD pin is used combinedly with the general-purpose I/O pin.
When host interface function is not used, please execute the pull-down of HIFMD pin.
Suitable Products
SH7619
SH7618
SH7606
  • 이 기사가 도움이 되셨나요?