메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to set the FWE using user mode and user program mode?

Latest Updated:03/23/2009

Question:

Is the transition of mode between the user mode and the user program mode possible only by the setting of the FWE pin?

Answer:

The transition of mode between the user mode and the user program mode is possible only by the setting of the FEW pin. Reset is not necessary.
Suitable Products
SH7124, SH7125
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086