메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to treat NMI pin of SH7615/SH7616 when NMI function is not used?

Latest Updated:02/07/2007

Question:

Please let me know how to treat NMI pin of SH7615/SH7616 when NMI function is not used.

Answer:

When NMI function of SH7615/SH7616 is not used, NMI should be pulled up at high level, in order that RES input makes "Power On Reset" operation.
Suitable Products
SH7616
SH7615
  • 이 기사가 도움이 되셨나요?