메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is internal access OK like access on-chip memory from CPU via C bus etc.?

Latest Updated:03/21/2012

Question:

Even when releasing bus outside, is internal access possible such as access to the on-chip memory from the CPU via C bus, and access to peripheral modules from the CPU via C bus, I bus, or P bus?

Answer:

Yes, internal access from CPU, DMAC and DTC is possible even in bus-right released state.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
  • 이 기사가 도움이 되셨나요?