메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is it possible to use #IRQ5 pin if the modem control signal is not used?

Latest Updated:03/23/2009

Question:

#IRQ5 input pin is allocated to the same pin as #CTS input pin (SCIF clear-to-send pin). When using SCIF, is it possible to use #IRQ5 pin if the modem control signal (CTS or RTS) is not used?

Answer:

Yes, It is possible. Please set SCFCR2.MCE bit to "0" and disable the modem signal.
Suitable Products
SH7729R
SH7727
SH7709S
SH7706